Part Number: INA241A
Other Parts Discussed in Thread: TPS61196, INA190, INA186
Dear Support,
for an Instrument OPAMP, I think both differential mode and common mode input resistance are very high, the current leakage to the ground can be ignored.
for this INA241A, it is a current sense amplifier, after it is inserted to the circuit, is the input bias current 35uA, equivalent to a 100K resistor connected to ground from the test point? assume the voltage of the test point is 3.5V.
is there a diagram to help understand this Bias current. what is the direction?
Thank you,
David