This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4192: Pspice Model (OPAx192) using single power supplies.

Part Number: OPA4192

Good Day.  The OPAx192 pspice model that was downloaded from TI.com has issues at times when running on a single supply (like 5V to ground).  it looks like it's taking time while computing bias levels.  Is there a recommended option setup you can recommend that might give better simulation times?  We are currently using Cadence 17.4 (Orcad Capture 17.4).  Output window shows the following:

Reading and checking circuit
Circuit read in and checked, no errors
Calculating bias point
Starting GMIN stepping
Starting power supply stepping
Starting pseudo-transient algorithm
INFO(ORPSIM-16594): To improve Pseudotransient Convergence and Performance, set following options to relax stabilization criteria for capacitor currents and inductor voltages: PTRANABSTOL=1e-5, PTRANVNTOL=1e-4
ERROR(ORPSIM-16550): Floating point computation failed during matrix solution. Possible solutions: 1)Ensure that all device parameters are in valid range. 2)Try using .options LIMIT
Divide by Zero, Divide
INTERNAL ERROR -- Divide by Zero, Divide
Run aborted
Total job time (using Solver 1) = 23.84

INFO(ORPROBE-3188): Simulation aborted

Thanks for your help.

John Gray