This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2197: Alternative to OPA2197

Guru 10680 points
Part Number: OPA2197
Other Parts Discussed in Thread: OPA2350, OPA2156

Hi, 

In one circuit, it was found that the slew rate of the OPA was slow and affected the measurement accuracy. So when OPA2197 with a high slew rate was used, an improvement in accuracy was observed. However, the margin of the terminal input/output current is low, so I am looking for an OPA that matches the other conditions.

Conditions
- Number : 2ch
- Slew rate : 20 V/us
- input/output current: ±10mA or more
- Package: SOIC - 8pin

As far as I can find, the maximum input/output current of TI's SOIC packages is ±10 mA. This is probably due to the internal diode clamping. If you know of any products that can flow more than 10 mA, please let me know.

Thanks,

Conor