This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi experts
i have some questions about TLV1805-Q1.
Q1:what is the output structure of TLV1805-Q1? are there any internal diode in IC?
Q2: the following is SCH from <TIDA-010071>.what is the aim of "14V SMAJ14CA"? to protect the TLV1805-Q1 output pin?
Q3: if "PILOT_out" short to 16V without D15, is TLV1805-Q1 damaged?
Hello Jay,
Q1: it is a standard complementary output consisting of N and P-channel NOSFET transistors.
The inputs and output are protected by ESD didoes to the supplies. These didoes are always there, even in shutdown.
Q2: The 14V SMAJ14CA is a bi-directional TVS diode to protect the circuit from external transients. External protection is always recommended when the signals come from "outside" the instrument.
Q3: R54 will limit the total current to ±12mA. The TLV1805 may get a little warmer, but it will not be damaged.
In a functioning system, the system should detect the short via the "PILOT_ADC" feedback monitor and throw an error flag (shut down).
Hi Jay,
10mA - same as the inputs. The ESD structures are similar.
But we recommend keeping the currents to below 1mA if possible. ESD diodes are not meant to continuously dissipate power.
if diode forward current max is 10mA, it seems like that ±12mA as you mentioned before will damage IC.
Hi Jay,
That is current trough the ESD diode - not the output.
The only way you would be pushing current through the diode is by forcing voltage greater than the supply into the output. The output cannot exceed the supplies on it's own.
The output can go up to 90-100mA peak (limited by thermal dissipation).