Part Number: INA213
Other Parts Discussed in Thread: INA210
In our application, we used INA210CQDCKRQ1,
The input signal is a PWM signal:
1) Freq=60KHz, Duty cycle=50%, Test VOUT=5V,
2) When reducing Freq=14KHz, Test VOUT is normal signal waveform.
Replace the INA213, and test the same phenomenon, that is at 60KHz, Test VOUT=5V.
May I ask if INA213/INA210 does not support 60KHz PWM input signal acquisition? What is the specific reason?
Are there any other recommended models? It is best to use PIN to PIN with INA210.