Part Number: LMH5401
Other Parts Discussed in Thread: THS4302,
Hi,
we are looking for an amplifier to use as as a differential to single-ended stage in a DAC signal processing chain. The amplifier must be high bandwidth (2 GHz minimum), DC coupled, and compensated such that it is stable at gains less than 5 V/V.
Initially we were considering the THS4302, but we decided this would be unsuitable in a difference amplifier configuration due to the problem of matching the internal feedback resistors. We also considered the OPA819, but this falls short of our 2 GHz bandwidth requirement. We are struggling to find unity gain compensated amplifiers that meet our requirements.
We came across the LMH5401 fully differential amplifier, which meets all our requirements by a decent margin and would be ideal for us if it were not an FDA, which brings me to my main question: Can we use an FDA such as the LMH5401 in a difference amplifier configuration? I've personally never seen this done before, which makes me think there must be some caveat that I've missed. The diagram below illustrates the configuration I'm considering (the actual resistor values and rails are yet to be optimized, I'm more concerned about the circuit topology at this point);
I've configured it as a difference amplifier by omitting the feedback on the non-inverting input and feeding the negative output to the next single ended stage, while ignoring the positive output (but still terminating it). From my simulations this configuration seems to perform reasonably well, with good CMRR. The performance doesn't seem to degrade much from the conventional differential amplifier configuration.
Any advice or wisdom on this would be much appreciated.
Thanks,
Jon