Other Parts Discussed in Thread: TLV7031, TLV7011
Hi,
I am using TLV3691IDPFR as an inverter to convert 3.3V to 0V or 0V to 5V. MCU MSP430F2274MRHATEP provides TTL control between 3.3V and 0V to feed TLV3691IDPFR. TLV3691IDPFR is biased with 5V so the output of TLV3691IDPFR swing between 5V and 0V.
When I use this comparator as an inverter and operate at -51C low temperature, I observer few seconds delay at output of pin#4. For example when I switch from 0 to 3.3V at pin#3, it takes few seconds for pin#4 to change from 5V to 0V. If I raise the temperature up to -40C or higher and the delay does not occur.
I verify TI's TLV3691 datasheet. On page1 it indicates industrial temperature range is -40C to 125C. However on page 4 absolute maximum rating is -55C to 150C.
My first question is: if few seconds delay is causing by running the comparator lower than -40C?
My second question is: Is the same device TLV3691 come with different package which can operate down to -51C? or any similar comparator with same package as TLV3691IDPFR I can drop in to replace without make design change? Please advise. Thanks.
Regards,
Lenny Lin