Part Number: LM2902
The following convergence error message comes up when I tried to model the LMX24_LM2902 as a single supply op amp.
INFO(ORPSIM-16594): To improve Pseudotransient Convergence and Performance, set following options to relax stabilization criteria for capacitor currents and inductor voltages: PTRANABSTOL=1e-5, PTRANVNTOL=1e-4
This issue was seen in a similar thread about three years ago but looks like the model still has the issue.
Here is a snippet of my circuit that I ran a bias point simulation for:
As mentioned in the other thread, the model works with dual supply where both voltages are the same. I was wondering if there was a version that had the fix. I can use TINA simulation tool but I just wanted to bring attention to this as it still seems to be a problem.