Other Parts Discussed in Thread: XTR117, , OPA192
Hello,
I am working on a design that is supposed to work from -55°C to +70°C and its storage temperature range is -60°C to +85°C.
I am using an INA826 as a bridge amplifier and the XTR117 for a current-loop.
But the INA826 is given to work from -50°C (instead of -55°C) and the XTR117 is given to be stored at the minimum of -55°C (instead of -60°C).
Does anyone know equivalents for those components which meet temperatures requirements ?
Thank you