This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI,
My name is Bryan from south korea...
I am using your products ina239 and ina239q series.
I would like to know whether the device ID of ina239 and ina239q products are the same.
If so, please tell me the dvice_id.
I will wait your reply...^^
Tks
As shown in section 7.6.1.17 in both datasheets, the device ID is the same (die ID 239h, revision 1).
Hi all,
Clemens is correct, the die id on both devices is the same at 239h. Thank you Clemens!
Tks a lot of your kindly reply..
I purchased 50pcs of PIN239Q on July 7, 2020 from ti web, and when I read the device ID of this IC, it reads as ina2390.
Then, I want to know if the device IDs of INA239, INA239Q and PIN239Q are different.
I want to know the MANUTURE ID and DEVICE ID of PIN239Q and then INA239 Id is INA2391.
The correct OPN for this device is INA239AIDGSR/T or INA239AQDGSRQ1.
The "P" prefix of "PIN239Q" indicates a prerelease device. Such devices are intended only for prototyping experiments; there is no guarantee that these devices are identical with the released devices, or that they work correctly. Apparently, some bugs were fixed between revisions 0 and 1.