Part Number: THS3491
Other Parts Discussed in Thread: THS3091
is the THS3491 unity-gain stable?
Or is there a better amp for that purpose?
Thanks and bye
Hanno
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hanno,
The THS3491 is not a unity-gain stable amplifier. The THS3091 is a current feedback amplifier that has similar performance, including the higher supply voltage range, that can operate in a unity-gain configuration.
If there are specific performance specs that you need for your application that the THS3091 does not meet, please let me know and I can recommend another part that meets those specs closer.
Thanks,
Nick
Well Hanno,
This table shows the suggested Rf vs gain for the 2 packages, the DDA has much higher bond wire inductance interacting with the loop phase margin, this went down to a gain of 2, but I would guess gain of 1 in the RGT would be stable for about 1.2kohm Rf, the sims will show what you need. I sort of set up the THS3491 definition assuming some gain since if you can produce an input signal with its slew rate for a unity gain case, why use the amplifier - hence the input headroom was relatively high to use a design giving better CMRR.