Part Number: INA181
Hi,
Best Regards.
I'm thinking of using the INA181 to convert a 4-20mA signal with an Rshunt of 3 ohms. This will result in a Voutput of 1.49V - 2.45V.
I would like to know if the INA181 is suitable for this purpose. Additionally, the idea is to have the PCB support 2-Wire (Loop current), 3-Wire, and 4-Wire connections. However, in the INA181 datasheet, I found the following information:

The 2, 3, and 4-wire connections look as follow:

In each scheme, my host board will provide power to the transmitter device.
Thanks in advance.