Part Number: INA333-Q1
Other Parts Discussed in Thread: INA333,
Hello, dear engineer;
The reason I use INA333: To measure the voltage difference induced on the coil. So the voltage difference will be very low. However, I have mentioned a few problems I encountered below:
1) I entered the values for the circuit which i designed and found the relationship between Vcm and Vo through the "Analog Enginner's Calculator" program.

After that simulated on Tına-TI. As you can see above if i use 'Vin+ = 120mV' and 'Vin- = 80mV', Vo will be 2.05V. But in my design, Vo is equal to 1.87V.


Therefore i try to solve problem and figure something. If i add Vref value to both Vin+ and Vin-, Vo will be 2.04V. But i did not see something about this on datasheet.


Hence, may i add VRef to inputs? How can i fix this issue? ( I am open-minded to your solutions.)
2) Ref pin needs to be a low impedance node (with source/sink in current low impedance output). But i do not have enough space on pcb. So instead of using designed that i mentioned above, using the design below may accure any future problems?

Thanks for your help.
Best regards,
Basri KAYA