This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, does TI have evaluation boards that would work for OPA2670 or OPA2673?
Hello Lance,
We do offer the DEM-OPA-RGV-EVM, which is an generic EVM board designed for VQFN (RGV) package PLC and DSL line drivers. The associated user's guide showcases the EVM functionality, which can do either two amplifier channels or a single differential output channel. Various sections of the OPA2670 & OPA2673 datasheets provide feedback resistor (Rf) values and other passive component recommendations.
If you would like help reviewing your schematic or component selection, please let me know. I can also assist with sending a DEM-OPA-RGV-EVM if you have trouble; however it is orderable on ti.com which will be the most efficient way to receive the EVM.
This DEM-OPA-RGV-EVM is unpopulated and blank, this is true for the majority of DEM-abc-xyz-EVM boards.
Best,
Alec
Hello Lance,
Please see the attached files.
AMPS160A(DEM-OPA-RGV-EVM)_Sch.PDF
AMPS160A(DEM-OPA-RGV-EVM)_BOM.xls
Best,
Alec