Part Number: THS4222
Other Parts Discussed in Thread: TLC074, OPA2690, OPA2890
Hi,
I need support about a simple circuit involving THS4222.
Attached you can see the circuit.
The input signal is a sinewave 3Vp 50Hz (0 offset), the output signal shows an offset (about 1.4V). Why?
What is the origin of this offset if the input signal has no offset?
I tried two simulators and the result is the same.
Thanks for your support.
Antonio