Part Number: TL081
Other Parts Discussed in Thread: LM741, TLV9301
Additional question.
I am also considering adopting LM741CN.
Please let me know the following information as it is not mentioned in the data sheet.
(1) When LM741 is used at -20°C to 80°C, what are the characteristics that deviate from?
(2) Output Current (RECOMMENDED OPERATING CONDITION)
(3)Temperature coefficient of input offset(TYP,MAX)
(4)Offset Voltage Adjustable Range
(5)Input Offset Voltage Null Circuit
thank you