Part Number: TL081
Other Parts Discussed in Thread: TL061, , TL031, TLE2021, UA741
Hello Ron Michallick
Thank you for your reply regarding TL031IP.
Please continue to answer the questions marked with "→".
>Is the supply voltage 24V (+/-12V); TL031AI is factory trimmed at 30V
→TL031IP is used at 24V (+/-12V).
> That would allow changing the Vos ; Does "Does it satisfy ±15mV (TYP)?" mean you want a high Vos?
→
(1) It is not intended for high Vos.
(2) I would like to know if it is possible to connect a 10kΩ trimmer resistor to the TL031IP and adjust it within the range of ±15mV (TYP) like the conventional products, UA741CP, and LM741CN.
Please tell me the ΔVIO(adj) (Offset voltage adjustment range) of TL031IP.
(3) Will connecting a 10kΩ trimmer resistor to the TL031IP and adjusting it cause the element to break?
(4) How is ΔVIO(adj) calculated?
>TL031, TL081 (not H), TL061 are all JFET. Concerns are staying in valid input common mode range, avoid step inputs.
→In the case of TLP031IP, how much value should I be careful about step input?
>TLE2021 may be a better solution; you have the option to remove potentiometer; this op amp has way better Vos and temperature drift. However input difference voltage is limited.
→TLE2021IP cannot be adopted because it is in "LIFEBUY" status in the data sheet.
Best regards