Part Number: INA280
Dear Specialists,
My customer is considering INA280 and has a question.
I would be grateful if you could advise.
---
This is a question regarding the TI device INA280A series.
I understand that the INA280 is a unidirectional current sense amplifier.
Could you please let me know what happens to the output when reverse current flows.
For example,
・0V (0A) output
・Undefined output
There was no plan to have the current flow in the opposite direction.
It is found a slight reverse current flows due to the capacitor and inductor on the load side.
At this time, I would like to confirm whether the detection circuit (control circuit) does not malfunction.
---
I appreciate your great help in advance.
Best regards,
Shinichi