Part Number: AMC3302
This is an item I inquired about three months ago.
"The input voltage specification for the AMC3302 is +/-50mV, but it is rated at +/-60mV from the shunt resistor.
Can I input the input signal by dividing it into resistors?
Of course, I believe that a better circuit can be constructed by mounting an operational amplifier on the input section,
but I do not want to prepare a power supply on the input side (primary side).
So please let me know if there is no problem with just resistor voltage division."
As a result of experimenting with the evaluation kit, it did not work properly. I would like to get some advice on
whether the number of circuits is inappropriate.