Part Number: AMC3302
The input voltage specification for the AMC3302 is ±50mV, but it is rated at ±60mV from the shunt resistor.
Can I input the input signal by dividing it into resistors?
Of course, I believe that a better circuit can be constructed by mounting an operational amplifier on the input section,
but I do not want to prepare a power supply on the input side (primary side).
So please let me know if there is no problem with just resistor voltage division.