Part Number: INA199
Hi,
In the circuit below, SENSE_H_CURRENT and SENSE_L_CURRENT were connected to INA199 input, and a load of 500 ohms was connected to +POWER.
The P+CAN voltage is approximately 11.8V, the INA199 input voltage is 5V, and the REF is connected to the GND.
At this time, INA199 output is about 55mV.
Is the normal output voltage correct?
If you connect a load of 20 ohms to +POWER, it's about 1.2V output.
It looks like a normal output, is that correct?