Other Parts Discussed in Thread: OPA855
I am designing a board with 4 OPA855 on a 4 layer board.
Looking at the evaluation board layout, it split the power plane and used the upper half for the positive(VS+) and the bottom half for the negative (VS-).
Now if I want to duplicate it for 4 OPA855, the power distribution looks messy.
How about I use the 4 layer board as below:
layer 1(top): components
layer 2: GND
layer 3: VS+
layer 4: VS-
on all layers just a whole copper pour and connect the supply through vias.
I have the following layout as the png attached.
I do not do the power plane split all the way from the input to the output SMA, instead, I only have some similar structure around the chip.
And for the C7 ((Johanson Technology) 500X14W103MV4T), how critical for it to be close to the chip? currently the layout that is close but overlap with the cutout at the output side, Should I move it further right to avoid that? And also the ground of the capacitor has to use via to the layer 2, is that a problem?
Thanks