This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you share input impedance of single ended signal P and N( not differential impedance)
.
Hello Abi,
I can check and see what I can provide about input impedance, common-mode, in addition to the 15 Ohm differential input impedance spec.
What circuit or end application would you be using the LMH6553 in? Do you have additional design questions?
Best,
Alec
Hello Abi,
The LMH6553 is an FDA (fully-differential amplifier). FDAs are a different than single-ended output op-amps and have a different input structure: you can think of FDAs as two inverting configuration op-amps which needed to have matched Rg and Rf (gain and feedback) resistors.
The Rg resistors on each input pin are primarily responsible for setting the input impedance of the FDA. Your design and Rg resistors will be the important pieces of your solution.
Best,
Alec