Other Parts Discussed in Thread: UC2845, LM2902, TLV9352, LM358LV
Dear Expert
We use LM2904DR as UC2845 flyback voltage control loop ,and we found in some batch LM2904 output nosie could be unormal .
This is our LM2904 voltage control loop sch ,IN- (PIN2)Input the voltage divider connected to a 2.5V reference source to 1.2V, IN +(pin3) conected the flyback output 3.3V and Out1(PIN1) conected the UC2845 VFB PIN to control the output voltage .
The UC2845 output 12V power GND will connected to LM2904 GND ,and UC2845 will have a 140k switch frequency .

Below is measure LM2904 IN and output waveform ,we found that 140K switch frequency will will interfere with the VIN pin through the ground wire, causing oscillations and unstable output loops. However, only a very small number of LOT batches will experience this issue, which has not occurred with machines produced in the past. May I ask if the anti-interference ability of our LM2904 varies among different batches.

Zoom in