Other Parts Discussed in Thread: OPA2994
Sir
We are planning to use the LM7322 to drive a MOSFET.
The operation condition is listed as follows
VS = + - 15V (Dual power supply)
VO = VGS = 2 ~ 3V
MOSFET = AOD496, Ciss = 1200pF_Max (as datasheet)
No resistive load connected at the output
Is it any risky to permanently destroy according to power dissipation across the output stage?
Regards
Ben