This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA277: OPA277 or LM741

Part Number: OPA277

How would you test for this op amp's open loop output impedance vs frequency and dc physically?  Are the inductor and capacitor there only for simulation or are small values needed in real life?  And how would you apply a current (with and without a frequency) to the output?  I tried it with a resistor and voltage waveform generator but it doesn't seem to be accurate.

  • The large value inductor and capacitor used in the output impedance over frequency simulation are there to isolate the output Zo from being effected by finite input impedance.

    In practice, you would apply at the output a small-signal IG1 sine current source (e.g. 100uA) at different frequency, 10mHz, 1kHz, etc. and back calculate, Ro=Vo/IG1, at any given frequency - see below. 

    For Zo measurement at 1kHz you could use 1H and 1mF as shown below BUT for lower values of LT and C1 the measurement will be corrupted my Zin. 

    OPA277 Zo.TSC

  • To clarify, to electrically measure this, you would have a voltage follower with a small current waveform at the output.  The capacitor and inductor are only needed for simulation.

    And for the current source at the output, are you able to use a voltage source/waveform generator with a resistor in series?

  • Please see below and attached presentation.

    The Great Zo Battle(v2).pptx