Other Parts Discussed in Thread: SN6501
Hi,
In ISO224EVM board the transformer used is 750313769.
The rated input voltage for transformer's only 3.3V. Whereas in Eval board the input voltage is +5V.

Even in datasheet of SN6501 the 750313769 is recommended for 3.3V to 5V application.
Could you please confirm whether the transformer 750313638 can be used for ISO224EVM ?

Regards,
Kannan