This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
Do we have rail-to-rail output performance device that can Pin2Pin replace OPA177? Customer need this spec to meet system requirement. Thanks in advance.
BRs,
Francis
The OPA191 and OPA192 are similar, but faster and CMOS. See this comparison.
Hi Jack,
Thanks for your help. Customer now need rail-to-rail in and out, so maybe the devices clemens mentioned will be more suitable.
BRs,
Francis
Hi Clemens,
Thanks for your help, could you please help me further understand the difference between Bipolar and CMOS? It is refer to the output structure, right?
BRs,
Francis
The architecture refers to all transistors, and this mostly affects the inputs. CMOS devices usually have lower input bias currents and power consumption and somewhat higher noise at the same speed; you see this in the comparison I linked to.
I do not know what characteristics are important in your application. In general, the differences of the OPA191/2 make them better, but a much faster amplifier might have more ringing at the output.
Hey Francis,
Please see our application note for an overview of the different input technologies (CMOS vs Bipolar vs JFET).
If customer needs RRIO, please suggest OPA191 which is a CMOS input amplifier. Notice the difference in voltage noise between the Bipolar Input Stage (OPA177) and CMOS Input Stage (OPA191). If the offset spec is not required, we also have OPA196 that is the low grade variant at 0.1mV offset voltage. Does 15 nV/√Hz voltage noise at 1kHz meet the customer requirement?
Regards,
Jack Snyder
Product Marketing Engineer | Precision Amplifiers