This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA296B-Q1: Use case of high value of series resistor at input path

Part Number: INA296B-Q1


Tool/software:

We need to monitor the current through a Shunt resistance of 40mOhm.

For the diagnostic purpose, we are planning to keep 1K ohm resistor in series between the IN+ & IN- pins and the shunt resistor.

So now the questions are,

1. Is it allowed to have 1K ohm resistance in front of IN+ & IN- pins of INA296B-Q1 device?

2. What is the functional impact of having high input resistance in front of IN+ & IN- pins of INA296B-Q1 device?

3. Is there any formula or simulation is available to estimate the impact of INA296B-Q1 device due to this configuration?