Other Parts Discussed in Thread: OPA2140, INA851, OPA2828, PGA855, OPA140
Tool/software:
The previous thread was locked.
I stacked another resistor network on OPA2140 feedback, and the CMRR improved. The unit is in uV/V
While this experiment shows the feedback network does affect the CMRR, the result is still off from the datasheet figure of ~32uV/V (-90dB) at 100kHz
Also, not every channel is this bad:These channels are with original resistor network values.
So I feel like this could be a device to device variation, just that it has quite a big spread.
Appreciate if the team can provide more insights.