Tool/software:
Hello there,
I am using TLV9004 opamp for one of my application, i am using it as a comparator without any hysteresis
My threshold set in inverting input is 2mV and my signal is ~6mV (for more than 35uS) at non inverting terminal, output of the comparator doesnt saturate properly, output slowly ramps towards 5V, when it nears ~100mV my input signal flips and ouput switches to '0'
when i subject this PCB to temp for 1 hour and measure the output of comparator reaches ~300mV, it stays in 300mV even after a day, is there a temp dependency in the opamp ?
Regards
Prince. A