Part Number: INA128
Other Parts Discussed in Thread: TL494
Tool/software:
INA128电路输入RC滤波、输入差分并联电容是否会影响其工作;
目前的电路图是否可以优化;
T want to ask Whether the INA128 circuit input RC filter and input differential shunt capacitance will affect its operation;
Whether the current circuit diagram can be optimized;
Schematic diagram


As shown in the figure above, INA128 is used for the output constant current loop sampling of the power supply;
INA128 differential output with RC low-pass filtering, as shown in the figure above, the loop appears obvious oscillation, and the FB waveform of the power chip is shown in the figure below:

INA128输出如下:
The INA128 output is as follows:

去掉差分输入的电容,电源芯片FB波形如下,波形比较稳定:
Remove the capacitance of the differential input, and the FB waveform of the power chip is as follows, and the waveform is relatively stable:

INA128输出,有比较大的开关噪声:
INA128 output, with relatively large switching noise: