Part Number: THS4031
Other Parts Discussed in Thread: TLC7524, THS3091, THS3491
Tool/software:
Hello, I need an alternative to THS4031ID with similar low settling time and low noise characteristics but with higher capacitive load drive capability. I am using it in inverting configuration with gain of -1.5 at the output of a DAC+OPAMP (TLC7524+THS4031ID) to drive a capacitive load of about 470 pF. For the TLC7524 DAC in unipolar operation I am using the same THS4031ID to generate 0V to -10V using REF102CU as the +10V reference. This 0V to -10V is being upconverted to 0V to +15V using the second THS4031ID.
I have observed some peaking response at the output load. Then I have used an isolation resistor and feedback compensation capacitor for the second THS4031ID and found the peaking and noise has reduced but the final 0V to +15V settling time has increased considerably. Is there any opamp I can use in place of the second THS4031ID which will not require any compensation or isolation circuit from the capacitive load and thereby retain the same settling time as the DAC ~500-600 ns? Please suggest.
Thank you