Tool/software:
Hi expert,
What is the output when the input is negative? Because the customer finds that OC protection is triggered for the system when there is a negative voltage on the input.
Thanks
Tool/software:
Hi expert,
What is the output when the input is negative? Because the customer finds that OC protection is triggered for the system when there is a negative voltage on the input.
Thanks
Hello Hangjie,
Thank you for your post.
Can you provide the schematic and scope shots of this negative voltage?
This will help me troubleshoot your issue.
Best Regards,
Joe
Hi Joe,
Thanks for your quick reply, i have send the sch via email, thanks.
Hello Hangjie,
Thank you for sending that over via email.
I noticed that C384, C385, and C836 are all the same capacitance.
This can cause issues so I would recommend either increasing the size of C384 by 10X or reduce C385 and C386 by a factor of 10.
Input Resistance Error for Current Sense Amplifiers
Please have them try this modification.
I hope this helps,
Joe