Part Number: INA745A
Tool/software:
Trying to evaluate INA745A. Having multiple issues, maybe related, maybe separate.
Hardware setup is TI SCB connected to INA745A EVB (SENS108_001 marked on PCBA, SENS109E1 marked on static bag it arrived in).
Using Windows 11. Following instructions on page 4 of INA740-INA741EVM, INA745-INA746EVM, INA780-INA781EVM User's Guide (Rev. A) (ti.com)
Downloaded and installed the PAMB driver. The SCB device shows up in Device Manager when plug it in, but it is a "Tiva Device Firmware Update."
I downloaded and installed the GUI, and as part of that, it offered to install the GC runtime, which I did.
Now when I run the GUI, it says "No SCB controller detected." I clear this error and then click on File -> Program Device. This fails with an error message and then it restarts the GUI.
When the GUI restarts, it says GC Runtime Installation Error.
The GUI is installed under the gcruntime.v12 folder.
I have tried everything I can think of to get past this.