This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Zhijun,
You can expect the input common mode voltage and output voltage swing specifications to be dependent on supply voltage. The required voltage drop across the transistors forces the amplifier to need some distance, or headroom, from each supply rail. For VICM, at higher supplies (such as your +/- 10V), the input headroom voltage to each rail will increase a bit from +/- 5V. Expect an input common mode swing around -8.75V to 9.25V, for a rough estimate.
We also have the THS2630, a new device with increased supply voltage and improved output swing specs.
Best,
Alec