This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA4230: Rail monitor future availability in QFN?

Part Number: INA4230
Other Parts Discussed in Thread: INA3221,

Tool/software:

I really like the INA4230/5 and wish to use it in future designs. It seems like a more capable successor to the INA3221 in every respect.

However I have one issue with it. The 16-DSBGA (0.71x1.47) requires 0.15mm/6mil capped via in BGA pad for the center pins.
This represents a board technology increase for my designs and would be the defining component for via size.

I am wondering if you have plans to offer this IC in a vqfn-16 or similar package for use in boards with lower tolerances / lower spec manufacturing processes.