This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The data sheet states that normally the part is set up where Vs+ is +5V and Vs- is ground. Can I use this with Vs+ = +2.5 and Vs- = -2.5?
I am also doing a DC input on the Vin+/Vin-
Both the spice models in PSpice and TINA seem to have problems (either convergence in Pspice or outputs fixed at -2.5V) in this configuration.
Regards,
Mark
Hello Mark,
You are able to use the THS7530-Q1 with split/bipolar supplies. It is likely a convergence and/or simulator issue with the SPICE model.
If you share your circuit I can take a look at simulating and see if I can find a small fix.
Section 10 of the datasheet details the ability to use split/bipolar supplies, as long as the total supply voltage does not exceed 5.5V.
Best,
Alec
Hello Mark,
I have not yet received the SPICE files. I am sending you a message with my email address.
I apologize, I am not sure why the file transfer did not work.
Best,
Alec
Hello Mark,
I am closing this thread as I am supporting via email. For the forum, the THS7530 model is designed to work in split supply and single-supply configuration. The model operates at a +/-2.5V supply configuration. Please be aware the model requires different design methodology than a typical voltage-feedback op-amp, as the THS7530 is a variable gain amplifier (VGA).
Best,
Alec