This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I ran a simulation using the model from this discussion :
At 125Hz:
Vout in theory:
Vout=f*C*R*Vcc=125*10*10E-9*47*10E3*3.3= 193.8mV
Vout from the simulation:
Vout= 183.1mV
Vout measured:
Vout=104mV
Can you tell me why there's a significant difference between the theoretical value and the experimental one?
Thank you in advance.