Part Number: THS3491
Tool/software:
1.What is the maximum output power of THS3491 under unlimited conditions?
2.If RL=100 ohms, single voltage supply 30V, frequency range 0-30MHz, HD2/3 is not considered, what is the maximum power output?
3. Regarding the second point above, if the actual line impedance is 100 ohms and a higher output power is required, can a transformer be used for impedance transformation to obtain a higher output power?
The maximum output power value under the condition of "unlimited conditions". Usually, the maximum output power is affected by factors such as power supply voltage, load impedance, frequency range, distortion requirements, etc. What is the actual maximum estimated power, or is there a rough calculation formula and method?