Part Number: THS3491
Other Parts Discussed in Thread: OPA817, , OPA810
Hi team,
we want to develop a 1000:1 high-voltage differential probe for the detection of high-voltage pulse signals. The maximum input is ±7kV, corresponding to the maximum output ±7V, and the signal bandwidth is more than 100MHz. The circuit topology is as shown below:

Now U1/U2 is ready to use OPA817 with high input impedance. Since OPA817 can only output about 3.5V, it cannot be used on U3. You need to find an op amp with an output greater than ±7V and a large and small signal bandwidth >100MHz. Please provide some selection and design suggestions.
Now I have initially found a THS3491. The large signal bandwidth meets the requirements according to the parameters in the specification. However, whether small signals below 100mV are OK is not clear from the specification. Please help confirm or recommend a more suitable model.