Part Number: TLV3501A-Q1
Other Parts Discussed in Thread: TLV9051, TLV7031-Q1
Tool/software:
Hi,
RT is NTC (TSM1D472H3953R01-8), the resistance value decreases as the temperature increases, requires the NTC to reach 85℃ ~ 100℃, the output low level, Turn the MOS off; after switching off, wait until the NTC has cooled to 60°C and put the output high.
Help calculate the resistance values of the surrounding using 3501a and 9051 respectively, and help to explain briefly the difference between these two operating devices in this case, thank you!

we hope that
The FET operates constantly on, and the Vout is high
FETs do not operate at all times off, Vout low
Best Regards
Ruoxin