Tool/software:
Hi TI,
I have to make sure that the circuit I design is properly protected against external electromagnetic field to meet EC standards.
Proper protection is particular important since wires to current sensing shunt can quite long, I would say up to 20m.
I would also like to achieve at least some overvoltage protection in case circuit is connected incorrectly.
Below is what I came up with. Does this diagram make sense? Can it be simplified?
TVS diodes are 600W peek power min.
Please advise.
Kind regards,
Thomas