This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear Team
We installed 100pcs of this device and found that the output was not functioning properly.
When we input 0V into the oscilloscope, the output should also be 0V, but the actual output reached 0.4V.
We conducted an ABA verification and found that the abnormal device was causing the issue.
Any suggestion on what I have mistaken or missed?
The circuit is:
The input:
The output:
Best regards,
Xiao
Hello Xioa,
100pcs of this device and found that the output was not functioning
Were all 100 non functioning?
In the output waveform the output is bimodal, what changes in the setup? (power on , off perhaps). What are the power supply voltages?
Try adding a 10pF or bigger capacitor in parallel with the feedback resistor to stabilize the feedback loop.