Part Number: INA232
Other Parts Discussed in Thread: TPS55288,
Tool/software:
Hey,
I am using the INA232 to measure current across my load from an external TPS55288 buck/boost and i wanted to know if the schematic is ok.
ISN Voltage is maximum 20V and the max curerent is being controlled at 3A from the TPS ISN/ISP pin.

X11-2 is exactly something like this 
And i would place a load resistor across those terminals.
Thanks