This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please show the schematic, and specify the supply and signal voltage ranges and the signal frequency.
It is likely that the desired output voltage is not far enough from the rails; see figures 7-12/7-13.
Hi User, Clemens,
I agree with Clemens in that we will need additional information about the circuit you are measuring.
Best,
Alex Curtis
Figure 7-36 shows that this should work when there is no load. As shown in figures 7-12/13, output voltages 1 V from the rails should work with 20 mA output current.
What is the exact voltage at which this happens? What is the load?
E2E user,
opa182-opa189-full-power-bw.pdf
best regards, Art
User,
The equation of Max Peak voltage can be expressed as follows:
VmaxPeak = SR/(2*pi*f);
if VmaxPeak >= Vpower_supply than VmaxPeak = Vpower_supply;
Assuming: Vsupply = ±5V, SR = 10V/μs, and f = 80kHz,
VmaxPeak = 10/(2*pi*f); = 10V/μs / (2*pi*80kHz) = 19.9V
since 19.9V > 5V, VmaxPeak = 5V.
Thus, at this frequency you should not expect slew induced distortion. Any distortion you see is due to loading effects or some other issue. You should disconnect the amplifier output to see if the distortion goes away.
I hope this helps.
Best regards, Art