This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV369: Negative Voltage measurement using ADC

Part Number: TLV369


Tool/software:

Hi everyone,

I'm trying to measure a -15V output from a DC-DC converter using the inbuilt ADC of an MCU, which operates on a 0-3.3V range. To scale down the voltage, I plan to use a TLV369 op-amp powered by 0V and 3.3V (no negative rail available, and I prefer not to add one).

How can I design the circuit to measure the -15V effectively with these constraints?