Tool/software:
Hey, I want to use the XTR117 to convert a 0-10V signal to a 4-20mA signal.
On my board, I have an Analog Voltage Output that provides a 0-10V signal, and on the same board, I have an Analog Current Input circuit that reads a 4-20mA current in a two-wire 4-20mA current loop configuration.
I am designing a testing jig where I can loop the Analog Voltage Output port to the Analog Current Input port, for which I require a converter circuit that I can attach in between.
How should I connect these, and what should be the value of RIN?
With Reference to this image.