Part Number: PGA308
Other Parts Discussed in Thread: XTR116, ADS1232
Tool/software:
I'm using a PGA308/XTR116 to convert a strain gauge output into 4-20mA.
Measuring the bridge voltage directly and calculating my offsets and gains seems to work well to give me 0.5 and 4.5V on VOUT of the PGA308 and then the XTR116 to translate that to loop current.
BUT, if I try to calibrate by measuring VOUT and back-calculate the bridge voltage (using the transfer function), it all goes haywire and my calculated offsets/gains sometimes cause the output to be shifted high or low and more often than not - saturated at 0 or 4.7V volts.
This could be because we are using such a tiny range of the strain gauge. Vs is 4.096V, the high-low delta across the bridge varies about +/- 4 to 7mV depending on the product configuration. Gains are typically in the 2000-3000 range.
I'm now looking at options to directly measure the bridge voltage to do the initial offset/gain calculations, then measure VOUT to do the fine tuning on ZDAC and GDAC.
I stumbled across the ADS1232. Would that be a good choice to measure the bridge voltages directly? The big package is a bit troublesome, but I may be able to make it fit.
Looking for recommendations for a good ADC to measure each leg of the bridge without causing any problems with the PGA308. Any advice from you gurus?