Part Number: TLV3501
Other Parts Discussed in Thread: LMV7239, TLC555
Tool/software:
I implemented this circuit. But I have a problem. I measure the value of the capacitor with a high-precision LCR meter. And then I insert it into its place in the circuit. When I power on the circuit and mathematically calculate the value of the capacitor over the frequency produced, I find a different capacitance value. In other words, there is a difference between the calculated value and the value I measured on the LCR meter. For example, the capacitor I measured as 102pF is calculated as 114pF. is it not normal to have such a big difference? I encounter this situation with different capacitors as well.
What is the problem?